Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LM5113-Slide12

Another challenge of a high reverse source-to-drain voltage is the potential of more losses during the dead-time. If circuit timing is not correct, the reverse conduction time can be too long, giving excessive losses or too short, giving cross conduction. A gate driver with separate input pins and matched propagation delays, allows either analog or digital tuning of the dead-time while the matched propagation delays maintain correct timing over a wide range of operating conditions. Shown in the scope shot is the switch node waveform with the dead-time minimized. Well matched propagation timing of the two channels is critical and users can see the negative peak is reduced.

PTM Veröffentlicht am: