Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
TMC5062 Dual Stepper Motor Slide 16

The UART interface can be operated with all standard baud rates, starting from 19200 baud. Depending on the TMC5062 clock frequency, up to 1 MBaud is permissible. The best range for the UART interface is 10 kBaud to 500 kBaud. As the interface automatically adapts to the master’s baud rate, no precise clock is required and no presetting of the baud rate.

PTM Veröffentlicht am: