Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Optoisolators Slide 4

The circuitry to the left shows an LED that transmits light through the light channel whenever a current passes through the input side. In the circuitry to the right, the light that is received on the output side triggers a current through the phototransistor or the Photologic® device, completing the transmission of information. The optoisolator allows power sources on both sides to be electrically isolated while transmitting information.

PTM Veröffentlicht am: