Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
key prod flexible

The two on-board mini PCIe card sockets accept a variety of plug-in modules such as Wi-Fi modems, analog to digital converters, GPS receivers, additional Ethernet ports, flash data storage, and other small sized plug-in cards for added flexibility. Both are full size sockets that provide PCIe and USB interfaces. One of the sockets also supports an mSATA interface. The SPI / SPX expansion connector allows low-cost analog and digital SPI interconnect expansion modules to be easily added to the system. SPX expansion that uses the SPI protocol provides an easy way to add low-cost, low-speed I/O expansion such as Analog Inputs or Digital I/O.

PTM Veröffentlicht am: