Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Common Mode Chokes Slide 14

On this slide a representation is shown of the frequency ranges in which the Würth Elektronik, Midcom common mode chokes operate. The WE-SL family of parts as seen in blue operate from the lower frequency spectrum, 10kHz, to the higher 10MHz side. This is due to the Manganese Zinc and Nickel Zinc materials used. These are targeted for DSL, Analog/modem applications, ISDN, CAN, Flexray, and Ethernet and USB applications. For moving from USB and Ethernet into LVDS lines, SATA, DVI and HDMI, the WE-CNSW product family, which utilizes nickel zinc materials, is optimum.

PTM Veröffentlicht am: