Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide10

Cross talk refers to the noise couple from any active conductor or signal line to any nearby conductor or quiet line. Forward or far end cross talk (FEXT) is the amount of noise at the output end of the cable that is induced on a nearby ‘quiet’ line. Factors affecting FEXT include pulse rise times and ground-signal conductor configurations (such as GSG, GSGSG etc). FEXT is specified as a percentage of the input pulse amplitude (for example, “a 5V signal with a 10% forward cross talk induces 5V on a nearby ‘quiet’ line”).

PTM Veröffentlicht am: