Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide5

The input pulse to a cable usually appears as in this model. There are three components to this pulse: Amplitude (or pulse height) refers to the voltage magnitude of the pulse. It is measured in volts in the vertical axis denoted ‘A’. Rise time (or pulse ‘turn-on’ time) refers to the length of time it takes the pulse to make the transition from the low or ‘off’ state to the high or ‘on’ state. Rise time (TR) is measured in the horizontal direction and expressed in nanoseconds. Width (w) (or duration) refers to the length of time a pulse remains in the high or on position. It is also measured in the horizontal direction and expressed in nanoseconds. As this input pulse travels down a length of cable, the three components will change.

PTM Veröffentlicht am: