Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
cable-Slide3

There are basically two types of signals that can be sent over a transmission line: analog or digital. Analog signals vary continuously in either amplitude or frequency. An example of an analog signal is a dimmer-controlled light: as the control is rotated, the intensity of the light slowly increases or decreases. The dimmer switch is actually varying the voltage amplitude of the output analog signal. The other type of signal transmission is digital. A digital signal has only two states: on or off. Digital transmissions are analogous to a light switch. Think of the eye as a receiver. As the switch which is flipped on and off, the eye sees the light flicker on and off. In the same way a digital signal is transmitted to a receiver conveying this same on-off information.

PTM Veröffentlicht am: