Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
eye 20
Tests conducted on the cable in the 3M Austin Laboratory produced a series of eye patterns. They show how the cable performs at different frequencies based on an eye opening of greater than 50% at different lengths, both with or without connectors. This pairing of eye patterns shows the performance of 0.25 m long with cable only as well as an assembly of the same length with connectors. The cable by itself offers 20 Gbps with a 73% opening, but even with connectors attached, it transmits 14 Gbps with 53% opening. For a ribbon cable, this is outstanding performance.
PTM Veröffentlicht am: