Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
eye 5
This pairing of eye patterns shows the performance of 0.25 m long standard 3749 Series Cable only and 7700 Series of the same length. At 5 Gbps, the standard cable is only able to offer a 29% opening. In contrast, the 7700 Series transmits 14 Gbps with 53% opening.
PTM Veröffentlicht am: