Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
eye 10
This pairing of eye patterns shows the performance of a 1.0 m long cable only, as well as an assembly of the same length with connectors. The cable by itself offers outstanding performance of 10 Gbps with a 50% opening, but even with connectors attached, it transmits 5 Gbps with 50% opening.
PTM Veröffentlicht am: