Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Wireless-Network-Slide16
In peer-to-peer mode an FFD can communicate to all other devices within its transmission range while an RFD can talk only to an FFD that it is currently associated with. Peer-to-peer mode is characterized by following properties: data frames can be delivered via several intermediate nodes (multi-hop transmission); large spatial areas can be covered by a single network; and complex packet routing algorithms are required. Note that the advanced functionality of the peer-to-peer mode is available only if an efficient network management protocol is realized on top of IEEE 802.15.4 stack.
PTM Veröffentlicht am: