Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Wireless-Network-Slide17
The IEEE 802.15.4 standard specifies only the lowest part of OSI communication model; the PHY layer and MAC sub-layer. The physical layer provides a means for bit stream transmission over the physical medium. The key responsibilities of PHY are: activation and deactivation of the radio transceiver; frequency channel tuning; carrier sensing; received signal strength estimation (RSSI & LQI); data coding and modulation; and error correction. The MAC sub-layer is responsible for reliable communication between two devices over direct physical link (without intermediate nodes). The key functions of the MAC layer include: data framing and validation of received frames; device addressing; channel access management; device association and disassociation; and sending acknowledgement frames.
PTM Veröffentlicht am: