Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide20
The CRA2512 series has excellent pulse characteristics for applications involving high inrushes of current such as a motor starting up. This chart shows measurements taken from a 140µs pulse with a maximum current of 82.5 A across a 100 mΩ resistor. Note that there is only a negligible change in resistance after the pulse.
PTM Veröffentlicht am: