Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide7
The signal is sent to the 50 Ω termination resistor, R1. Because of load matching, the signal is dissipated safely with a minimum amount of back reflections. In this way the amplifier will still operate at 50% of capacity. Also, if the destination of the amplified signal is off line (for example a damaged antenna), the amplified signal will travel backwards through the coupler to the termination R2 to ground safely without damaging the amplifier.
PTM Veröffentlicht am: