Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
basics contd
The three basic components in the construction of a joystick are the handle, rubber boot, and a mounting nut/bezel. The handle is the primary user interface, while the boot protects the switch from environmental exposure, and the mounting nut/bezel is used to hold the joystick in place after mounting to a panel.
PTM Veröffentlicht am: