Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
micro tech
The microswitches used in the design of these joysticks have either an on or off position, and do not have a proportional output such as that found on resistive based joysticks. Image 1 (left) shows that as the lever is moved there is no change in output until, after a few degrees, it will turn the North switch on. Image 2 (middle) shows when the lever is not moved, it is central to the switch, not touching any of them and therefore no contact is made. Image 3 (right) shows the opposite to image 1, as the lever is pulled fully in the opposite direction, the South switch will be activated.
PTM Veröffentlicht am: