Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
SiC-Schottky-Slide20

Snubber circuits often required by traditional silicon boost diode designs can be eliminated by the use of a Wolfspeed SiC Zero Recovery diode. The result is a significant reduction in component count and improved airflow. The circuit diagram on the left shows a silicon diode in a PFC application and the necessary snubber circuitry. SiC Schottky diodes are used on the right, so no snubber circuitry is needed. Less component count improves Mean Time Between Failures (MTBF), and lowers the Bill Of Materials (BOM) cost.

PTM Veröffentlicht am: