Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
SiC-Schottky-Slide8

The graphs in the upper right hand corner of this slide provide a comparison of reverse recovery characteristics. The waveforms illustrate the turn-off, or diodes switching from forward bias conducting mode of 10A current to reverse bias. It also shows the off state intervals of a SiC Schottky diode, and an ultrafast soft recovery silicon diode at the junction temperatures of 25, 50, 100, and 150°C. Since SiC Schottky diodes are majority carrier devices which do not have a recombination process during turn-off, there is no reverse recovery current during turn-off.  SiC Schottky diodes reverse characteristics are also independent of forward bias current and junction temperatures. This is illustrated by the red line on the graph.

PTM Veröffentlicht am: