Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
SiC-Schottky-Slide6

The PFC control block modulates the boost converter so that the input current of the power supply will be in phase and have the same wave shape as the input sine-wave voltage. As the wave shape and phase are aligned, the supply is said to achieve near unity power factor. The DC/DC converter, usually a step-down converter, steps the high dc voltage down to output voltages required to run the system’s electronics. The DC/DC circuitry also provides  primary to secondary isolation while the output filter stage blocks switching noises from the power supply. 

PTM Veröffentlicht am: