Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
XB-D White LEDs Slide 13
Another advantage of the small size and lumen density of the XB-D is that it can reduce the physical size of the reflector as can be seen on this page. Using a smaller reflector  lowers the system costs. This is particularly advantageous compared to the arrays that are available in the marketplace. In addition, with discrete LEDs it is much easier to make trade offs in lumens and lumens per watt by simply adding or removing discrete LEDs as necessary.
PTM Veröffentlicht am: