Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
XB-D White LEDs Slide 15
This chart details the standard order codes for the XB-D LEDs binned at 85° C. Also shown, in the column at the right, are the flux values at 25° C which is where nearly all power LEDs are binned and thus would be the flux values to use when comparing the XB-D to the competition.
PTM Veröffentlicht am: