Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
True Reverse Current Block Continued 2

True reverse current blocking is usually required for USB power path applications to avoid unwanted reverse current for all cases. The scope trace demonstrates this operation. The first section shows an initial state normally ON or VIN = VOUT without a load. The second section shows a transient higher voltage applied at VOUT inducing a reverse current creating a voltage drop from VOUT to VIN which reaches threshold for VT_RCB. After the time interval tBLANK the PMOS is turned OFF blocking the reverse current as shown in the third section. Please note that TRCB activation requires transient or continuous reverse current, which can develop voltage drop > VT_RCB. If VOUT > VIN and is applied slowly, then reverse current charges input capacitor and VIN will follow VOUT without TRCB activation.

PTM Veröffentlicht am: