Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Undervoltage Lockout

Undervoltage Lockout ensures the proper behavior of the Load Switch within a specific range of input voltages. Each subsystem within the switch has operational voltage limitations therefore it is desirable to allow switch operation only in a known good range applicable to all systems. The specific voltage at which the part works properly resides between UVLO min rise and UVLO max rise. The part is definitely in lockout when VIN is below this minimum and definitely working when past the maximum. A small area of uncertainty resides between the two voltages. Once the device is operational the trip points for lockout voltage change to some lower values as shown on the right side of the chart. There is a hysteresis component shifting the voltage to limit the possibility of oscillation.

PTM Veröffentlicht am: