Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Practical Resistor Values

This shows the position of the RLIM resistor used to program the current and the practical current range is from 125mA for the high values to 2.6A for the low value. Caution will be needed if exceeding 2A due to thermal considerations. Overcurrent for the non-A devices place the power switch into a current liming mode. The A types are latched off with an overcurrent event.

PTM Veröffentlicht am: