Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
automotive-slide9

As mentioned on the previous slide, EPCOS has the standard DC Link that was originally developed to give an alternative to aluminum electrolytic capacitors when the customer is looking for a higher reliability and longer life product. The capacitance range of the original series was 10µF to 110µF with voltage rating up to 1100 VDC. With the expansion to the Brick type, the maximum capacitance has been increased to 480µF and the voltage rating to 1300 VDC.

PTM Veröffentlicht am: