Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
X2Film-Slide6
As previously discussed, to reproduce the harsh conditions to which capacitors may be subjected when assembled in an external meter application, the following test conditions have been standardized: a humidity level of 85% rH, 85°C temperature, and 290 VAC for a duration of 1000 hours with a maximum capacitance drift of ±10%. In the diagram shown, the heavy duty demonstrates very stable performance compared to the standard series that after 100 hours started to show excessive degradation.
PTM Veröffentlicht am: