Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
transponder-slide6

The main applications of transponders coils include: immobilizer systems which create a stop command, passive entry / passive start (PEPS) which enables activation without physical key connection (push button start) and tire pressure monitoring (TPMS) which measures the pressure of the air in the tires. The key factor is the short distance RF systems operating at 125kHz.

PTM Veröffentlicht am: