Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
transponder-slide8

This slide explains the product offering for passive entry / passive start, otherwise known as PEPS, applications. The product range covers the complete spectrum of components that are needed to create an integrated user experience. Key fobs are required to work differently in several spacial enviroments executing unique command depending on where they are at any given point in time. For example, TDK offers the completed customized antennas for door handles, interior, and trunk allowing for keyless access and remote functions. Moving towards the driver entry position executes a different set of commands and options(open one door, open all doors, open trunk). Once inside the compartment of the vehicle ignition functions and smart location allow for the user to avoid locking the keys in the vehicle.

PTM Veröffentlicht am: