Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
flash mem
The QG8 and QG4 offer respectively 8Kb and 4Kb of flash. They utilize the third-generation flash with the low-voltage programming option, proven out on the GB/GT60A. Whereas the first S08 families only allowed programming down to 2.1V, the flash on the QG allows programming all the way down to 1.8V. This is a key feature in helping eliminate components of the board, saving money and board real estate.
PTM Veröffentlicht am: