Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
ser comm port
The 16-pin version of the QG family offers all three standard types of serial communication ports. In addition, they are all available for use in parallel, rather than multiplexed with each other which could limit system options and, potentially, applications. One important note on the IIC is that the spec mentions operation “up to 100kbps”, but that considers maximum bus loading and timing. With reduced bus loading, the IIC can achieve higher baud rates.
PTM Veröffentlicht am: