Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
quarter brick chart
Starting with OmniOn Power's quarter brick modules, there are four Barracuda high powered modules, the PIM400 power entry filter module, and the Hammerhead high powered module in a quarter brick package. Any part number starting with the letter “Q” signifies a quarter brick package. The numbers embedded in the middle of the part number signify the maximum output current capability, while the letter at the end signifies the output voltage. In this case, “B” represents 12 VOUT. As an example, the QBDW033A0B is a 33 AOUT, 12 VOUT quarter brick. Notice that OmniOn Power's Barracuda modules are offered with either a digital or an analog interface. If the module has a “D” in the part number it calls out the digital version. A “V” in the part number calls out the analog version.
PTM Veröffentlicht am: