Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
HLSR-Slide3

The HLSR is the first, from the ground up, current transducer utilizing LEM’s second generation ASIC. It is very compact for a transducer capable of supporting 150A continuous current. This ASIC contains all the electronics in the transducer including the hall cell. The HLSR is a galvanically isolated device capable of measuring AC or DC current. It is available in two mounting styles, through hole or surface mount.

PTM Veröffentlicht am: