Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
HO8-Slide13

Shown on this slide is a comparison between generation one HG1 and the generation two HG2 ASICs. Some of the advantages are: the reference out voltage has more flexibility, the reference input voltage can be pulled lower with the HG2 giving even more dynamic range for unidirectional measurement applications, the response time is 2.5x better, offset drift and gain drift are roughly half, and noise density is approximately 25% less.

PTM Veröffentlicht am: