Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
HO8-Slide8

The HO series is available in three fixed current settings. The 8, 15 and 25A versions are further adaptable using the three separate bus bars allowing for a broad range of measurable currents. This device has a low-power mode feature for use in electronics requiring a sleep mode. The HO performs a self test continuously and outputs the results on the EEPROM control active pin. On the pre-programmed models the OCD is set to 3x nominal current.

PTM Veröffentlicht am: