Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
HO8-Slide3

The HO is an ASIC based transducer. This ASIC contains all the electronics in the transducer, including the Hall cell. The HO is a galvanically isolated device capable of measuring AC or DC current. It has an over current detection (OCD) pin that makes it unique. The HO is available in two mounting styles, through-hole or surface mount.

PTM Veröffentlicht am: