Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

In today’s high speed networks, the capacitive loading that the SIDACtor presents to the signal is also of some interest. The capacitance of a SIDACtor is dependent on three things. First off, the selected VBO will determine the capacitance. This is a chart of the nominal capacitance of a SIDACtor in the popular C rated MC series. As seen above, when selecting a SIDACtor with higher VBO, the basic capacitance of the device decreases.

PTM Veröffentlicht am: