Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

Once the SIDACtor device is in crowbar state, the current through the device must go below the holding current in order for the device to reset into its off state. From an application standpoint, this means that the holding current should be higher than the current that could be provided by the protected system. This is one reason SIDACtor devices are found being used mostly in limited power systems such as telephone, data and signaling.

PTM Veröffentlicht am: