Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

VBO is the breakdown voltage of the SIDACtor device. When VBO is applied to the device, it switches into the crowbar state. Between VDRM and VBO, a SIDACtor device will behave much like a TVS diode clamping device. VBO varies considerably from device to device and will increase slightly as the device’s temperature is increased.

PTM Veröffentlicht am: