Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
KMT32B Magneto Resistive Sensor Slide 3

The KMT32B is a magnetic field sensor based on the anisotropic magnetoresistance (AMR) effect. In essence, the AMR effect consists of sensing the magnetic field direction independently of the magnetic field strength for applied field strengths of H>25 kA/m. The sensor contains two parallel supplied Wheatstone bridges which enclose a sensitive angle of 45 degrees.

PTM Veröffentlicht am: