Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
KMT32B Magneto Resistive Sensor Slide 6

This illustrates the basic operation of the KMT32B. A rotating magnetic field on a surface parallel to the two Wheatstone bridges (x-y plane) will deliver two independent sinusoidal output signals, one following a cos(2α) and the second following a sin(2α) function where “α” is the angle between the sensor and field direction (see Figure 2). With this data, both the angle of the magnet and the linear position can be determined.

PTM Veröffentlicht am: