Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Switches Slide 18

AquaMEC is a solution to get IP 67 sealing from the front panel. A boot with a sealing in between is mounted on the front panel to create the IP 67 sealing. The solution also has an illumination possibility where the cap and the boot are transparent and the illumination can be seen not just from the top but also from the side.

PTM Veröffentlicht am: