Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Switches Slide 8

On the left side of this slide, there are the dimensions for 5E/5G through-hole and surface mount versions. In the middle, there is the 5G switch with illumination. In the case of two LEDs, the polarity of the terminals 2 and 3 are reversed to shift between the LEDs. The 5 series switches have three standard actuation forces. In order to distinguish them better, the actuator of the 2.0 N is grey, the 3.5 N is black, and 6.5 N is blue.

PTM Veröffentlicht am: