Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Switches Slide 5

These two windows explain the assembly order of UniMEC™ accessories. The LEDs and lenses are pushed into the bezel and are added to the switch simultaneously. It is important with the alternate version that the actuator is in the upper position when dismounting the accessories, as well as during soldering in order to keep the functionality of the switch. As mentioned earlier, UniMEC has 8 contact functions which can be seen in the wiring diagram.

PTM Veröffentlicht am: