Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Accelerator-Slide11

The SPI interface of the VTI automotive series is designed to support almost any microcontroller that uses software implemented SPI. The accelerometer operates always as a slave device in the master-slave operation mode. The data transfer between the master and accelerometer is performed serially with a four wire system in 16-bit frame. SPI protocol has measurement error indicators and it supports burst mode reading.

PTM Veröffentlicht am: