Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Accelerator-Slide8

The sensor element and signal path are tested by deflecting the proof mass of the sensing element to both directions over a predefined dynamic range. The test is done automatically during start-up and it can be repeated by a CTRL-register command. The result of the test is a momentary mass deflection seen in the output of the device.

PTM Veröffentlicht am: