Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Roard-Level Reliability (BLR)

The LFPAK56D half-bridge comes with all the known LFPAK benefits. Board-level reliability being one of these, the LFPAK package allows for thermal expansion when the module temperature fluctuates during operation, especially in thermally-demanding powertrain applications. This is unlike QFN packages which do not allow for any movement, meaning cracks in the solder joints which potentially result in electrical failures.

PTM Veröffentlicht am: