Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Half-Bridge Value Proposition

The true benefit of the half-bridge is around the reduction of tracks on the PCB. In the example here on the left is a dual MOSFET. To make a high side and low side connection, one would route under the board to make the S1D2 connection between the two MOSFETs. This adds additional inductance into the design and can impact the ground plane as well as the thermal paths. In the case of the half-bridge, the connection is made internally using Nexperia’s innovative packaging technology, removing the need of the connecting track on the PCB. This supports lower system level inductance and offers a simple plug-and-play solution for design engineers.

PTM Veröffentlicht am: