Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 30
The first part of the image illustrates the operation of PWM0 in continuous mode. The rising and falling edges of PWM0 are controlled by the 16-bit counter and match the active and deactive registers. The match active register defines the position of the rising edge while the MTCHDEACT register defines the falling edge of the waveform. The PWM output changes when the 16-bit counter matches the values defined in the related registers. The SYNC_IN input of each PWM timer is used to reset (resynchronize) the PWM block. The SYNC_OUT can be asserted immediately after the SYNC_IN or can be delayed via the SYNDEL register. In the second part of the image, PWM0 is synchronized with PWM1. Each time a sync event is provided to PWM0, PWM1 starts or restarts after the sync delay programmed in the SYNDEL register. The image on this slide illustrates the Timer 1 carrier signal with a 50% duty cycle modulated with the internal PWM. The modulated signal typically has a higher frequency.
PTM Veröffentlicht am: