Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 44
The following are the steps that would be carried out by a non-nested ISR: push all registers that are used (according to the ARM-Procedure-Call Standard) on to the stack, determine the interrupt source by reading the INT_VECTOR register, and execute the ISR. Pop all saved registers back from the stack. Finally, end the ISR by restoring the Program Counter register (PC). Now consider the extra steps needed for nested routines. After finding the interrupt source, raise the priority-masking threshold to the priority level of the interrupt request to be served and re-enable interrupts in the processor. From this point, only interrupt sources with a higher priority level than the current interrupt source can interrupt the core. Then, execute the ISR. After completion, restore the saved priority mask and follow the remaining steps.
PTM Veröffentlicht am: